Setup Text
Show the oscilloscope's setup information.
- In the Screen Image view, the setup text will only be shown after the "Get Current Screen" button is clicked.
- In the Trace Data view, the setup text will only be shown after the Get Current Trace mode is selected and the "Start" button is clicked.
Below is an example of setup text that shows the analog, math, reference waveform, digital, trigger, horizontal, and acquisition settings.